DWL@DWL10000551527
Verze | Jazyk | Operační systém | Datum | Velikost | Typ | Stáhnout |
---|---|---|---|---|---|---|
3.0.0 | EN | 06.07.2023 | 474 MB | ZIP | HMI_Service_Center_3.0.0.zip | |
Popis |
HMI Service Center Update Paket The HMI Service Center is software for testing B&R industrial PCs and Automation Panels. Testing covers different categories such as COM, network and SRAM. Since version 3.0.0, the HMI Service Center is available as a free download. The HMI Service Center update package (SCU file) can be used to update an HMI Service Center USB flash drive. The update is performed with the HMI Service Center Maintenance tool. Changes - Removed copy protection. The HMI Service Center can be used at no cost starting with this version on. - Added support for APC4100. - Added support for SMART values of NVMe disks. - Added support for SMART values of RAID volumes. - The network test has been optimized for slow connection establishment. - Updated the B&R company logo. - Testing LED "HDD" on devices equipped only with a RAID volume or M.2 option is no longer performed since this is not technically possible. |
|||||
Verze | Jazyk | Operační systém | Datum | Velikost | Typ | Stáhnout |
2.0.0 | EN | 05.07.2021 | 422 MB | ZIP | HMI_Service_Center_2.0.0.zip | |
Popis |
HMI Service Center Update Paket The HMI Service Center is software for testing B&R industrial PCs and Automation Panels. Testing covers different categories such as COM, network and SRAM. The HMI Service Center update package (SCU file) can be used to update an HMI Service Center USB flash drive. The update is performed with the HMI Service Center Maintenance tool. Error corrections - In the event of an unforeseen restart (e.g. voltage loss), test execution was resumed at the second-to-last test instead of the last test. - During the storage test, the SMART attributes were displayed several times during a multiple test run. - The HMI Service Center USB flash drive could not be used for the USB test in automatic test mode with multiple test runs. Changes - Changeover to 64-bit WinPE. - At least 2 GB RAM is required for execution. - Support for UEFI boot. - Support for MPC3100. - Support for PPC900 TS17 CPU boards. - Support for PPC1200. - Support for M.2 modules (5ACCMS01.MDT2-000). - Support for IF modules 5AC901.I232-00, 5ACCIF02.CANE-000, 5ACCIF02.ISS0-000, 5ACCIF02.FPLS-000. - UPS and CPU temperature are no longer additionally displayed during the temperature test. - Improved texts for SRAM and touch screen test. - Removed support for APC510, APC511 and PP500. - Removed support for APC810 and PPC800. - Removed buzzer test since it is no longer possible in the 64-bit version. - Removed function "Beep on error" since it is not longer possible in the 64-bit version. |
|||||
Verze | Jazyk | Operační systém | Datum | Velikost | Typ | Stáhnout |
1.10 | EN | 13.07.2018 | 303 MB | ZIP | HMI_Service_Center_V1.1.zip | |
Popis |
HMI Service Center Update Paket The HMI Service Center is a software tool used to test B&R Industrial PCs and Automation Panels. The test covers various categories such as COM, network, SRAM, etc. The HMI Service Center update package (SCU file) can be used to update an HMI Service Center USB flash drive. The update is performed with the HMI Service Center Maintenance application. Error corrections - When exiting the HMI Service Center on an unknown device, an error message appeared stating that the data could not be serialized. - The resolution was not set correctly for displays connected via VGA. - The third USB interface could not be tested on APC510. Changes - At least 1 GB of RAM is required for execution. - Support for APC910 TS17 CPU boards. - Support for APC2200 and PPC2200. - Support for APC3100 and PPC3100. - Support for AP1000 and AP5000. - Support for SDL3 and SDL4. - Support for SDL4 Converter. - Support for IF network cards 5AC901.IETH-00 and 5ACCIF03.CETH-000. - Support for module functions on APC910, APC2100, APC2200, APC3100, PPC900, PPC2100, PPC2200 and PPC3100. - Panel fan speeds are no longer displayed. - Display of factory settings during fan test. - Company name changed. |
|||||
Verze | Jazyk | Operační systém | Datum | Velikost | Typ | Stáhnout |
1.00 | EN | 13.07.2018 | 244 MB | ZIP | HMI_Service_Center_V1.0.zip | |
Popis |
HMI Service Center Update Paket The HMI Service Center is a software tool used to test B&R Industrial PCs and Automation Panels. The test covers various categories such as COM, network, SRAM, etc. The HMI Service Center update package (SCU file) can be used to update an HMI Service Center USB flash drive. The update is performed with the HMI Service Center Maintenance application. Changes - First edition. |